Issue:
How to order a custom assembled pendant station
Product Line:
Push Buttons and Operator Interface
Environment:
XACA pendant stations sold and supported in the USA.
Resolution:
Add -9 to the enclosure part number and submit a keysheet with the order. For example: XACA04 custom assembled is order as XACA049. XACA06 is ordered as XACA069.
How to order a custom assembled pendant station
Product Line:
Push Buttons and Operator Interface
Environment:
XACA pendant stations sold and supported in the USA.
Resolution:
Add -9 to the enclosure part number and submit a keysheet with the order. For example: XACA04 custom assembled is order as XACA049. XACA06 is ordered as XACA069.