{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do HVL and HVL/cc switches meet UL 1062 ?
Issue:
HVL and HVL/cc switches meet UL 1062 standard

Product Line:
Medium voltage switchgear.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Yes. Both switches comply with the requirements of UL 1062, which is the standard for Unit Substations. They also comply with our Unit Sub UL File E216538 which is a UL 1062 listing file.


Schneider Electric Canada