{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I order a key operated push button such as catalog number 9007KR137 with a key other than the standard E10 type key?
Issue:
Identify a part number for a key for a selector switch

Product Line:
9007 Harmony 30mm Push Buttons and Selector Switches

Environment:
Push Buttons and Operator Interface

Resolution:
To order the key operated push button using a non standard key number, such as an E11 key, add the key number after the catalog number as in: 9001KR137E11.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: