{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What type branch breakers does a Mini Power-Zone (MPZ) indoor/outdoor packaged power supply with a ``B`` after ``MPZ`` use? An example of which is an MPZB7S40F.

Article available in these languages: Spanish

Issue:
Selection of branch breakers for MPZ and MPZB

Product Line:
LV Transformers

Environment:
Applies to Mini Power- Zone (MPZ) Transformers by SquareD/Schneider Electric

Cause:
Branch breakers for MPZ and MPZB products are customer supplied

Resolution:
The MPZ with a bolt-on interior, also referred to as a ``MPZB``, can accommodate Type QOB bolt-on breakers and  can also still accommodate Type QO plug-on breakers.  Thus, you can use both QO and QOB breakers in the MPZB!

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: