Issue:
What are the dimensions of an MA1000R circuit breaker enclosure?
Product Line:
PTFDS - FD Enclosure Systems
Environment:
Circuit breaker enclosures sold and supported in the USA.
Cause:
Dimensional information on MA1000R.
Resolution:
The physical dimensions for a MA1000R are 52.08`` high, 21.64`` wide, 9.82`` deep. Refer to on-line drawing #3100, link below.
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.
What are the dimensions of an MA1000R circuit breaker enclosure?
Product Line:
PTFDS - FD Enclosure Systems
Environment:
Circuit breaker enclosures sold and supported in the USA.
Cause:
Dimensional information on MA1000R.
Resolution:
The physical dimensions for a MA1000R are 52.08`` high, 21.64`` wide, 9.82`` deep. Refer to on-line drawing #3100, link below.
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.
Released for:Schneider Electric Canada