{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the maximum conductor length for EBA, EMA, XDSE, and ASCO Surge Suppressors?

Issue:
What is the maximum conductor length for EBA, EMA, XDSE, and ASCO Surge Suppressors?

Product Line:
Surge suppressors

Environment:
TVSS EBA, TVSS EMA

Cause:
Installation

Resolution:
To obtain the maximum system performance, locate the device as close to the circuit being addressed as possible to minimize the interconnecting wiring length. For every foot of wire length, approximately 160 Volts (6 kV / 3 kA, 8/20 microsecond) is added to the suppressed voltage. The Voltage Protection Rating (VPR) is located on the device nameplate and is measured six inches from the enclosure sidewall, according to UL® 1449 test standards.

Schneider Electric Canada