{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the part numbers for the different wireway extension kits for the NQ and NF panels?
Issue:
Parts Kits

Product Line:
NQ NF Panelboards

Environment:
Products sold in North America

Resolution:
The following are for NEMA 1 surface mount applications only.  Boxes must be MH type 20 inch wide x 5.75 inches deep.

Extension kits include the cover and are available from 4 inches to 60 inches.  RTI part numbers are ordered with the prefix WW and the required length.  Example: WW4 is the 4 inch wireway, WW12 would be 12 inch etc.

All are in 1 inch increments. Anything above 60 inch must be ordered as factory assembled.





Schneider Electric Canada