{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can a viewing window be provided on a double throw safety switch?

Issue:
Can a double throw switch be provided with a viewing window in the cover?

Product Line:
Safety Switches

Resolution:
Viewing windows allow visible indication of the blade position in the switch without opening the cover. Double throw safety switches, 30-100 A, with a DT or DTU catalog number prefix can be provided with viewing windows, factory installed only. Add suffix VW to the catalog number. Viewing windows will be provided for both top and bottom ON positions.

Schneider Electric Canada