{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the part number for the armature assembly for the 8536SG series A starter?

Issue:
8536SG Series A (no coil voltage given) -what is the part number armature assembly for this starter.

Product Line:
NEMA Type S Starters and Contactors

Environment:
North American Products

Cause:
​Would like to replacement the artmature for a size 5 series a starter

Resolution:
If your contactor or starter is a Class 8502/8536 Type SG Series A and you need to replace the armature and magnet assembly, purchase one of the following E-Coil Conversion Kits. These kits include a magnet, armature and the new electronic coil along with fusing. Replacement Series A armature/magnet kits are not generally available. If it is a 600v or jogging application, contact Control PSG.

E-Coil Conversion Kits For Series A

Class 9998 Type SG120 - 120VAC
Class 9998 Type SG208 - 208VAC (Obsolete)
Class 9998 Type SG240 - 240VAC
Class 9998 Type SG380 - 380VAC (Obsolete)
Class 9998 Type SG480 - 480VAC

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: