{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Panelboard screw part number 2159017081, what is the thread size. Also thread size for part number 4020513001K.
Issue:
Thread size for screw part number 2159017081 and 4020513001K.

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
2159017081 is a 10/32 x 1/4`` , 4020513001K is a 10/32 x 1/2``

Schneider Electric Canada