Search FAQs
Do the 8501C Power relays meet UL924 ratings?
Issue:
Do the 8501C Power relays meet UL924 ratings?
Product Line:
General Purpose Relays
Environment:
Square D Power Relays
Cause:
Customer is looking for a relay that meets UL924.
Resolution:
No. UL 924 is a standard developed by Underwriter`s Laboratories covering Emergency Lighting and Power Equipment. This standard was developed to help guide the use of electrical emergency related equipment and, in the case of emergency egress, works hand in hand with the Life Safety Code (NFPA 101). This standard directly addresses exit sign construction, visibility, and use.
Do the 8501C Power relays meet UL924 ratings?
Product Line:
General Purpose Relays
Environment:
Square D Power Relays
Cause:
Customer is looking for a relay that meets UL924.
Resolution:
No. UL 924 is a standard developed by Underwriter`s Laboratories covering Emergency Lighting and Power Equipment. This standard was developed to help guide the use of electrical emergency related equipment and, in the case of emergency egress, works hand in hand with the Life Safety Code (NFPA 101). This standard directly addresses exit sign construction, visibility, and use.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: