{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you put the LA4DWB on two LC1D09G7 contactors and still put a mechanical interlock between them also?
Issue:
Mount a mechanical interlock on LC1D contactors with LA4DWB

Product Line:
IEC Contactors and Starters

Environment:
Tesys D Contactors

Resolution:
Yes you can. You have to use the LAD4BB adapter on both contactors to mount the LA4DWB, but because they are mounted near the rear of the contactors, and flush to the contactors, the mechanical interlock can still be mounted also.

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: