{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the cover / padlock attachment for a key operated 9001KR pushbutton?
Issue:
Identify the part number for a padlock attachment for a 30mm pushbutton

Product Line:
Harmony 30mm Push Buttons and Accessories

Environment:
Push Buttons and Operator Interface

Resolution:
The 9001K108 is a cover type attachment that can be padlocked to keep unauthorized personnel from tampering with the operator. The 9001K109 is the same as 9001K108 but with a spring loaded lockout cover.


CTA-ID : 2047713

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: