Issue:
Product Design Features
Product Line:
J Frame Circuit Breaker Enclosures
Environment:
Service Entrance Ratings
Cause:
Application
Resolution:
Yes. The Powerpact J frame enclosures are all marked 'Suitable for Use as Service Equipment' (USA ONLY) when the solid neutral assembly is installed.
NOTE:
For Service Entrance use in Canada, see the current Canadian Digest pages for the circuit breaker enclosures.
Search FAQs
Are the J-Frame Enclosures (J250F, J250S, J250R, J250DS, J250SS and J250AWK) Suitable for use as Service Equipment?
Released for:Schneider Electric Canada
Explore more
Product:
Explore more
Product: