Search FAQs
What enclosures are available for a PowerPact P-frame circuit breaker?
Issue:
Enclosures for Powerpact P-frame (80% and 100% rated)
Product line:
Molded Case Circuit Breaker
Resolution:
The PowerPact P-frame breakers have several enclosure options:
800 A maximum options are M800S (NEMA 1), M800R (NEMA 3R), M800AWK (NEMA 12), and M800DS (304 grade stainless steel) or M800SS (316 grade stainless steel; both NEMA 4,4X,5)
1200A maximum options are P1200S (NEMA 1), P1200R (NEMA 3R), and P1200AWK (NEMA 12)
100% rated P frame PowerPact breakers, 800 A maximum, can be used in all of these enclosures.
Enclosures for Powerpact P-frame (80% and 100% rated)
Product line:
Molded Case Circuit Breaker
Resolution:
The PowerPact P-frame breakers have several enclosure options:
800 A maximum options are M800S (NEMA 1), M800R (NEMA 3R), M800AWK (NEMA 12), and M800DS (304 grade stainless steel) or M800SS (316 grade stainless steel; both NEMA 4,4X,5)
1200A maximum options are P1200S (NEMA 1), P1200R (NEMA 3R), and P1200AWK (NEMA 12)
100% rated P frame PowerPact breakers, 800 A maximum, can be used in all of these enclosures.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: