{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a B phase modification kit for NQ B phase hi-leg panels to enable putting a three pole breaker in the panel?
Issue:
B phase modification kit for NQ B phase hi-leg panels to install a three pole breaker

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
NQ B phase high leg panels must be ordered as factory assembled. Three pole spaces should be called for if three pole breakers are to be added in the future. B phase high leg panels ordered with all single pole spaces cannot be modified in the field.

Schneider Electric Canada