undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can the coiled neutral pigtail wire on a QO-GFI, QO-CAFI, QO-DF, QO-SWN, HOM-GFI, HOM-CAFI, HOM-DF, or HOM-SWN breaker be shortened? Will that affect its performance?
Issue:
Can the length of the pigtail wire of a QO or Homeline GFI, AFI, CAFI, DF or SWN breaker be shortened or lengthened?

Product Line:
QO and Homeline Circuit Breakers

Resolution:
The coiled neutral pigtail wire may be shortened or lengthened as needed using approved wiring practices.
In all applications, the pigtail must be connected to the neutral bar.

Schneider Electric Canada

Can the coiled neutral pigtail wire on a QO-GFI, QO-CAFI, QO-DF, QO-SWN, HOM-GFI, HOM-CAFI, HOM-DF, or HOM-SWN breaker be shortened? Will that affect its performance?
Issue:  
Can the length of the pigtail wire of a QO or Homeline GFI, AFI, CAFI, DF or SWN breaker be shortened or lengthened?

Product Line:
QO and Homeline Circuit Breakers

Resolution:
The coiled neutral pigtail wire may be shortened or lengthened as needed using approved wiring practices.
In all applications, the pigtail must be connected to the neutral bar.

Schneider Electric Canada
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
Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top