{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for a 100% copper neutral kit for the NF panelboard?
Issue:
Part number for a 100% copper neutral kit for the NF panelboard

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Maintenance.

Resolution:
The 100% copper neutral kit for the NF panelboards are:
100A and 125A use NFN1CU, the 250A use the NFN2CU and the 400/600A use NFN6CU


CTA-ID : 2048749

Schneider Electric Canada