{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why can the 480V delta system not be used on NF panelboards?

Article available in these languages: Spanish

Issue:
480 Vac Delta systems incompatibility with NF panelboards

Product Line:
Panelboards

Environment:
NF panelboards

Cause:
Application, Installation, Rating

Resolution:
The EDB branch breakers used for NF panels have a maximum single pole voltage of 277V. On a 480V delta system, a single pole would see 480V which is more than the branch breakers are rated for.

Schneider Electric Canada

Explore more
Range:
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Category: