{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the Form for ordering a combination starter minus the open starter?

Issue:
Form used on combination starters to order it without the Starter.

Product Line:
NEMA Contactors and Starters

Environment:
8538, 8539 Combination Starter

Cause:
Form Code Identification

Resolution:
Form Y188 can be used to modify a combination starter so that it ships without the starter.  The unit will only have the box, disconnect, and any other control/relay options installed.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: