{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are trim and dead front screws for NQ, NQOD & NF panels, up to 250 amps, the same type of screw?

Article available in these languages: Spanish

Issue:
Trim and deadfront screws for NQOD, NQ and NF panels

Product Line:
Circuit breaker panelboards and accessories sold and supported in the USA.

Environment:
Maintenance

Cause:
Determine of type of screws used in circuit breaker panelboards.

Resolution:
NQ and NQODmono flat (225A and less) and NF (250A and less) trims = 40205-130-01K.
NQ and NQOD and NF trims for 400A and higher = LP9502
All NQ, NQOD and NF hinged trims = LP9502 and 40205-130-01K
All TVSS trims, equipment space trims and contactor covers = LP9502
All deadfront screws = 80025-067-01

Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: