{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is included in the NQMB2Q adapter kit and how is it installed?
Issue:
Contents of the NQMB2Q kit and how to install

Product Line:
NQ Panelboards

Environment:
Products sold in North America

Resolution:
The NQMB2Q Main breaker kit for the Powerpact Q frame Mains contains: Main circuit breaker deadfront cover (1), main circuit breaker mounting pan (1), deadfront support brackets (2), ``Main`` circuit breaker label (1), 10-32 x 7/16 inch tapping screws (2), 10-32 x 5/16 inch tapping screws (6), 8-32 x 2 1/4 inch tapping screws (2), 8-32 x 3 1/4 inch tapping screws (2), Main lug wires + neutral, qty (4). Main Lugs qty (4) P/N NQALM2

Note the Installation Instruction Guide attached

Schneider Electric Canada

Attachment(s)
NQ-Q-Frame Main Circuit Breaker (225 A Maximum) and Adapter Kit Installation 80043-722-02.pdf [7.14 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top