{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What alarms are possible to show with the M2C and M6C programmable contacts?

Issue:
What are the protective functions (alarms) to show with programmable contacts?

Product Line:
Molded Case and Air Circuit Breakers

Resolution:
Alarms can be enabled or disabled for protection or load shedding. When an alarm occurs, an entry is made in the alarm log. The following features are available:
1. Ir Long-time pickup
2. Ii Instantaneous pickup
3. Isd Short-time pickup
4. I Ground-fault current
5. AI Ground-fault alarm
6. Iunbal Current unbalanced
7. Iamax Phase A demand overcurrent
8. Ibmax Phase B demand overcurrent
9. Icmax Phase C demand overcurrent
10. Inmax Neutral demand overcurrent
11. Vmin Voltage is below set minimum
12. Vmax Voltage is above set maximum
13. Vunbal Voltage unbalanced
14. rPmax Reversed power
15. Fmin frequency is below set minimum
16. Fmax Frequency is above set maximum
17.  Phase rotation
18. Ished Current shedding
19. Pshed Power shedding
20. Not Selected No alarms selected

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: