{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What amperage of QO tenant breaker can be used with the EZM125QOA tenant breaker adapter kit?

Issue:
Product Features

Product Line:
EZM Metering

Resolution:
Due to the short circuit current ratings (SCCRs) of the EZM metering equipment, when the EZM125QOA adapter kit is used, it will accept ONLY 2p, QO (40 to 125 A), QO-VH (40-60 A), or QOH (40-60 A) tenant circuit breakers.

The installation instructions for the EZM125QOA will state "USE ONLY 2 POLE 125A MAXIMUM CIRCUIT BREAKER QO, QO-VH OR QOH", but for the SCCR of the EZM metering equipment, the above must be followed.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: