{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the 30-60-100 amp fusible bus plug for both the 3-wire and 4-wire devices fit on both 3-wire and 4-wire busway?
Issue:
Can 3 phase 3 wire plug in units for busway plug inot 3phase 4 wire busway?

Product Line:
busway plug in units

Environment:
I-line and I-line II busway

Resolution:
Yes. When a 3-pole plug-in unit is installed on 4-pole busway, there is no neutral connection. This is most often done when a 3-wire load needs to be feed from 4-wire busway. When a 4-pole plug-in unit is installed on 3-pole busway, the neutral stab makes no connection. This can be done, but it would only be considered if a 3-pole device was not readily available.

Schneider Electric Canada