{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are 48 volt replacement control coils available for LC2D12004?
Issue:
Identify a replacement for an IEC contactor's coil

Product Line:
Class LC1D Contactors

Environment:
IEC Contactors and Starters

Resolution:
This coil is obsolete. Replace the contactor with the new TeSys product, LC2DT25E7. Note this is a functional equal only. Accessories for the old product may or may not fit the new design. Confirm dimensions.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: