{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is a main upper housing assembly for a 8502SE or 8536SE?
Issue:
Upper housing assembly replacement for NEMA size 3 contactor and starter

Product Line:
Contactors and Starters

Environment:
NEMA Contactors and Starters

Resolution:
31074-112-51, complete upper housing assembly excluding armature, magnet, control coil and cover. For starters manufactured after February 1992.
31074-539-50, complete upper housing assembly including the armature, magnet, and cover. Excludes the control coil. Will also update starters made prior to February 1992.

Schneider Electric Canada