{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the plastic cover that swings out on an MCC Model 6 that holds the Start/Stop pushbuttons, 22mm or 30mm?

Issue:
Replacement Part

Product Line:
Motor Control Center

Environment:
MCC6, Model 6

Cause:
Door for control units

Resolution:
Advised customer that for the 22mm 5 device Control station panel, replacement part number is 80420-007-05. For the 30mm 3 device Station control panel, replacement part number is 80420-007-06. In either case the cover will be blank with perforated cut outs in the back. This a replacement part and cannot be added to an existing bucket that did not come set up to accept control devices.

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: