{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What lugs are included in lug kit CMELK4 and what are their mounting torque specification?
Issue:
Product Feature

Product Line:
Metering Accessory

Resolution:
CMELK4 is a lug kit that includes a quantity of (4) TA-600-2N, ILSCO mechanical lugs.
Wire range of the Ilsco TA-600-2N lug is #2 AWG to 600 kcmil Al/Cu, and torque value for wire binding screws is 375 lb-in (inch-pounds).
Lug mounting hardware as used in most metering equipment includes (2) 1/2"-13 keps nuts (part number: 23427-02800), and (2) flat washers (part number: 23601-00282) per lug. Bag assembly 4056211850 includes (6) keps nuts and (6) flat washers.
Torque value for 1/2"-13 keps nut is listed on each unit's wiring diagram, typically 300 lb-in (inch-pounds).

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: