{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you wire the shunt trip on a EDB breaker?
Product Line:
PowerPact E frame

Environment:
Applies to EDB, EGB, and EJB with shunt trip accessory installed.

Resolution:
Use terminals 6 & 7 on the breaker to wire the shunt trip. Because it is AC, it is polarity insensitive. The other terminals are not operative.



For more information please see instruction bulletin 48840-097-02.

Schneider Electric Canada