{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a neutral assembly for the QO200TRNM Enclosed molded case switch?
Issue:
Product Design features

Product Line:
Enclosed Molded Case Switches

Resolution:
No, a solid neutral assembly is not available for this device. This device is rated single phase, 2 wire, 240 Vac max.

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: