{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the NQ panels come pre-filled with filler plates?
Issue:
Filler plates included with NQ panelboard

Product Line:
Panelboards

Environment:
NQ Panelboards

Cause:
Product features

Resolution:
Factory ordered NQ panels will come with filler plates installed in all empty spaces.

NQ RTI panels from 18-42 circuits come with one bag of 15 filler plates with the hardware bag. NQ panels 72-84 circuits come with 2 bags of 15 filler plates for a total of 30 plates. Order additional filler plates as needed with part number NQFP15 (1 pack = 15 fillers).

Schneider Electric Canada