Issue:
Replacement fuse base for 9422TCF33
Product Line:
Operating Mechanisms and Disconnect Switches
Environment:
9422 disconnect switches
Resolution:
The complete fuse base assembly is a 31301-058-52. This will include the fuse clips and lugs. This switch uses Class H, J, K or R fuses. The Class R rejection clip is not included. To convert to Class R clips, also order RFK06.
Replacement fuse base for 9422TCF33
Product Line:
Operating Mechanisms and Disconnect Switches
Environment:
9422 disconnect switches
Resolution:
The complete fuse base assembly is a 31301-058-52. This will include the fuse clips and lugs. This switch uses Class H, J, K or R fuses. The Class R rejection clip is not included. To convert to Class R clips, also order RFK06.