{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the dimensions for the J250F and J250S circuit breaker enclosures?
Issue:
Dimensions

Product Line:
Circuit Breaker Enclosure

Resolution:
Both enclosures are 31.00" H x 14.00" W x 5.96" D.
The J250F flush cover is 32.50" H x 15.42" W.
The J250S surface cover is 31.43" H x 14.35" W.

See drawing at the following link: https://www.se.com/us/en/download/document/3362S/

The drawing is also attached.


Schneider Electric Canada

Attachment(s)
3362S.pdf [98.23 KB]
Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: