{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the interior mounting studs for an I Line HC4259DB box field replaceable ?
Issue:
Replacement Interior mounting studs for an HC4259DB box

Product Line:
I Line Panelboard

Environment:
Installation

Resolution:
The replacement mounting studs are 1/2-13 and threaded, P/N 80025-040-01, The keeper nut is  P/N 23304-02801.
NOTE : Install Studs from the back of the box.

Schneider Electric Canada