{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can a two pole I-line frame breaker be used for a single pole application?

Issue:
Can a 2 pole I-line breaker be used as a single pole breaker?

Product Line:
Circuit breaker

Environment:
I-line breakers

Cause:
Application

Resolution:
Yes, only one pole on the breaker can be used since both poles have a common trip.  The breaker will still work properly.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: