undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Does the FFTK report generator software work with the Windows 7 or Windows 10 operating system?
Inquiry:
Can the FFTK report generator software for testing Micrologic trip units FFTKRPT-V1-0 (FFTKRPTV10) be used with Windows 7, Windows 8, or the Vista operating systems?

Product Line:
Micrologic trip units for Powerpact M, P, R frame and Masterpact NW and NT

Resolution:
The Report Generator software will not work on Windows 10.
It will work on Windows 7, 8, and Vista, but not if you use the default directory provided with the software. Please use the following work-around:
In order for the FFTK report generator to function properly, you need to have it installed it in a write-accessible folder on your system. Most “new” versions of Windows (Vista, 7, 8) have special permission control on the [C:\Program Files (x86)] and [C:\”Program Files”] folders. On these newer systems, we recommend installing the FFTK report generator to somewhere where you have write permissions such as…
For all users of the system: [C:\Users\Public\”Public Documents”\”FFTK Report Generator”].
For a single user: [C:\Users\{USER_NAME.EN_US}\”My Documents”\”FFTK Report Generator”], where {USER_NAME.EN_US} is the desired user.

See attachment to download the Report Generator software.

Schneider Electric Canada

Attachment(s)
FFTK Report Generator (1) (1).zip [7.12 MB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.