{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference between the 8903LO06 and the 8903LO60?
Issue:
How to read 8903L lighting contactor poles from the part number

Product Line:
NEMA and Definite purpose contactors and starters

Environment:
Class 8903 Type L Lighting contactors

Resolution:
The 8903LO06 is a Multipole Lighting Contactor with 6 Normally Closed Power Poles
The 8903LO60 is a Multipole Lighting Contactor with 6 Normally Open Power Poles

The first digit corresponds to the NO power poles, the second digit corresponds to the NC Power poles

NOTE: If part number includes 4 numbers, the first two digits are the NO and the last two the NC

Schneider Electric Canada