{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the P1200S, P1200R, or P1200AWK circuit breaker enclosures approved for use with 100% rated P frame PowerPacT breakers?
Issue:
Product Design Features

Product Line:
Circuit Breaker Enclosures

Resolution:
The P1200S, P1200R, and P1200AWK enclosures are tested and listed for use with 100% rated P frame PowerPacT breakers up to 800 A maximum.

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: