Search FAQs
What is the difference between the J250S and JD250S circuit breaker enclosures?
Issue:
Product Features
Product Line:
Circuit Breaker Enclosure
Resolution:
The JD250S is physically smaller than the J250S and has application limitations. The JD250S is UL listed only to accept an HDL or JDL 3 pole circuit breaker. The voltage is limited to 480 Vac maximum. The SCCR is limited to 18 kAIC at 240 Vac or 480 Vac. Copper conductors must be used.
Product Features
Product Line:
Circuit Breaker Enclosure
Resolution:
The JD250S is physically smaller than the J250S and has application limitations. The JD250S is UL listed only to accept an HDL or JDL 3 pole circuit breaker. The voltage is limited to 480 Vac maximum. The SCCR is limited to 18 kAIC at 240 Vac or 480 Vac. Copper conductors must be used.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: