{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the TVS120XR80S or TVS120XR80S be connected to function on a 120V 2-wire + G system?
Issue:
Can the TVS120XR80S or TVS120XR80S be connected to function on a 120V 2-wire + G system?

Product Line:
Surge Protection.

Environment:
Products sold in the United States.

Cause:
Application.

Resolution:
Yes, in a single-phase, 120-volt, 2-wire application, connect both SPD black wires to the same line.
XR Wiring Diagrams

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: