{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a 100% rated HDL or JDL circuit breaker be installed into a JD250S enclosure?
Issue:
Application

Product Line:
Circuit Breaker Enclosures

Resolution:
This enclosure has been tested and listed for use ONLY with standard rated (80%), 3p HDL or JDL breakers.
NOTE: The voltage is limited to 480 Vac maximum. The SCCR is limited to 18 kAIC 240 Vac or 480 Vac. Copper conductors (75°C) MUST be used.

Schneider Electric Canada