{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What type secondary fuses are used in MCC starter units with control transformers?

Issue:
Replacement secondary fuse in a control transformer in an MCC Nema starter

Product Line:
Model 6 MCC's and accessories

Environment:
Maintenance/selection

Resolution:
Secondary fuses are FRN-R type fuses
120V 50VA CPT- .5 amp 25413-00060
120V 100VA CPT- 1.0 amp 25413-00090
120V 150VA CPT- 1.6 amp 25413-00130
120V 300VA CPT- 3.2 amp 25413-00190
120V 500VA CPT- 5.0 amp 25413-00230

Schneider Electric Canada