{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the lug rating for the 200% rated neutral for a NQ non linear load 225A panel or the neutral kit NQNL2?
Issue:
Lug rating for the 200% rated neutral for a NQ non linear load 225A panel or the neutral kit NQNL2

Product Line:
Panelboards.

Environment:
Products sold and used in North America

Cause:
Product features.

Resolution:
The lug rating is 1 - #6 - 350KCMIL AL/CU per lug. The non linear load panel has 2 of these incoming lugs per panel.

Schneider Electric Canada