{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many ZB2BE contact blocks can be put behind an operator in an XACA enclosure?
Issue:
Determine the number of contacts that fit inside a XACA enclosure

Product Line:
Harmony 22mm XACA Push Button Stations

Environment:
Push Buttons and Operator Interface

Resolution:
You can only mount 2-ZB2BE101 or 102 contacts behind a single button in this enclosure. You can not stack these because of the enclosure depth.

Schneider Electric Canada