{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the ZBZ3605 and ZBZ16** guards keep the operator in the in depressed mode when padlocked?
Issue:
How can an operator stay in the depressed mode?

Product Line:
22mm Push Buttons

Environment:
XB4 Padlockable guards

Cause:
Determine if the guard is locked in the depressed position for an application

Resolution:
Yes, that is the only way to get the device padlocked. Also they must be used with the listed trigger action mushroom buttons. It is not however lock out tag out certified. It is only a control device.

Schneider Electric Canada