Issue:
Needing information on the acceptable room temperature for the SR2 and SR3 Zelio Smart relays
Product Line:
Relays and Timers
Environment:
Zelio™ Logic Smart Relays
Resolution:
-20 to +55 °C or -4 to +131 °F free standing or -20 to +40 °C or -4 to +104 °F in enclosure.
Needing information on the acceptable room temperature for the SR2 and SR3 Zelio Smart relays
Product Line:
Relays and Timers
Environment:
Zelio™ Logic Smart Relays
Resolution:
-20 to +55 °C or -4 to +131 °F free standing or -20 to +40 °C or -4 to +104 °F in enclosure.