Issue:
Can the QONQ30LS400 QONQ42LS400 QONQ42MS300 QONQ42MS400, be installed in a MH-WP, NEMA Type 3R, Rainproof enclosure?
Product Line:
QO Load Center
Environment:
300A and 400A QONQ
Resolution:
The 300A and 400A QONQ Load Center Interiors are UL Listed only for use in NEMA Type 1 enclosures. For a NEMA Type 3R application, consider using the NQ panelboard product line.
Can the QONQ30LS400 QONQ42LS400 QONQ42MS300 QONQ42MS400, be installed in a MH-WP, NEMA Type 3R, Rainproof enclosure?
Product Line:
QO Load Center
Environment:
300A and 400A QONQ
Resolution:
The 300A and 400A QONQ Load Center Interiors are UL Listed only for use in NEMA Type 1 enclosures. For a NEMA Type 3R application, consider using the NQ panelboard product line.