Search FAQs
Are the 9001BR* Nema 7 & 9 hazardous location enclosures water proof?
Issue:
Clarify if 9001BR stations rated Nema 7 & 9 are also waterproof?
Product Line:
Control Stations and Enclosures, Nema 7 & 9.
Environment:
9001B Standard Duty Control Stations, Class 1, Division 2, Groups B,C, or D. Class 2 Division 1 and 2 Groups E, F or G.
Resolution:
No, NEMA 7 & 9 enclosures are explosion proof, but not water or air tight.
Clarify if 9001BR stations rated Nema 7 & 9 are also waterproof?
Product Line:
Control Stations and Enclosures, Nema 7 & 9.
Environment:
9001B Standard Duty Control Stations, Class 1, Division 2, Groups B,C, or D. Class 2 Division 1 and 2 Groups E, F or G.
Resolution:
No, NEMA 7 & 9 enclosures are explosion proof, but not water or air tight.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: