{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the 9001 Type SKS key operated selector switch available?
Issue:
9001 SKS key operated selector switch availability

Product Line:
Push Buttons and Operator Interface

Environment:
9001SK Corrosion Resistant Selector Switches

Resolution:
No, it is not available. There is an error in the 175 Digest that lists keyed selector switches, but they are not valid.

CTA-ID : 2051170

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: